1 Reply Latest reply on Jul 31, 2019 1:18 PM by e14softwareuk

    Can't Select and Modify Wires but Components are selectable

    rpruitt76

      Have an interesting problem. Well more frustrating...On one of my schematics, I can't select or modify my wires. I can place additional wires but one they are placed, I can't move them or select them. The problem is more bizarre in that if I open the same schematic file from another Laptop running another variant of Circuit Studio, that package has full access to my wires and can select and modify them.

       

      Suspect Laptop running Circuit Studio under Windows 10 is running version 1.5.2 (Build 30)

       

      Laptop running Circuit Studio where wires are selectable is also running Windows 10 running version 1.2.0 (Build 37)

       

      Any advice would be greatly appreciated.

       

      Thanks