2 Replies Latest reply on Sep 12, 2019 8:12 AM by tomdeboerio

    Error in final lauch sequence

    tomdeboerio

      Hi,

       

      I am trying to install a debugger with Eclipse for my project on a MKV58F1M0xxx24. I am running Eclipse from a Virtual Box environment running Ubuntu 16.04 (64 bits).

      I followed all the instructions in https://gnu-mcu-eclipse.github.io/debug/jlink/  to install the tools. Currently, I am able to compile my project, and to load it in the target through command line by using the following commands:

         JLinkExe -device MKV58F1M0XXX24 -if swd -speed 4000

         JLink>r

         JLink>loadbin <filename>.bin,0x10000000

       

      From those tests, I can tell that my JLink tools are correctly installed outside of Eclipse.

      When I try to debug with Eclipse, the compilation works correctly, but I am getting the following error when the debugger connects to the target

       

      I am sure I messed up somewhere in my set-up, but the fact that it seems to be able to connect correctly to the target, then crash has me confused.

      Any ideas I could try ?

       

      Regards

      Tom