1 Reply Latest reply on Sep 20, 2019 4:46 PM by ilg

    Eclipse debug session - dropped 'gdb' connection

    mikej_w

      I'm close to having this work - but the GDB connection gets dropped - like this:

       

      GNU MCU Eclipse OpenOCD, 64-bitOpen On-Chip Debugger 0.10.0+dev-00593-g23ad80df4 (2019-04-22-20:18)

      Licensed under GNU GPL v2

      For bug reports, read

      http://openocd.org/doc/doxygen/bugs.html

      Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

      adapter speed: 2000 kHz

      adapter_nsrst_delay: 100

      none separate

      srst_only separate srst_nogate srst_open_drain connect_deassert_srst

      Started by GNU MCU Eclipse

      Info : Listening on port 6666 for tcl connections

      Info : Listening on port 4444 for telnet connections

      Info : clock speed 2000 kHz

      Info : STLINK V2J29S7 (API v2) VID:PID 0483:3748

      Info : Target voltage: 3.183290

      Info : stm32f4x.cpu: hardware has 6 breakpoints, 4 watchpoints

      Info : Listening on port 3333 for gdb connections

      Info : accepting 'gdb' connection on tcp/3333

      Info : device id = 0x10076413

      Info : flash size = 1024 kbytes

      Info : flash size = 512 bytes

      Info : dropped 'gdb' connection

      shutdown command invoked

       

      Any ideas on how to fix this? Thanks in advance!

      Mike