1 Reply Latest reply on Sep 25, 2019 4:22 PM by bhfletcher

    which bsp to use for PicoZed FMC Carrier Card v1

    openhacker

      I want to build petalinux on FMC Carrier Card v1.

       

      I've already built bare metal applications successfully (I used board definitions for Vivado 2016.04, and then imported them into 2018.3

       

      The board defintions I see on:

      PicoZed FMC Carrier Card v1

      look like they're for FMC2 (I assume that means V2?)

       

      There's older bsp's which don't even list FMC1 (I assume at FMC1 there was no "versioning"?)

       

      So, since I've never done this before (can I construct a bsp from a baremetal application which runs in the SDK?), where do I get a "good"

      bsp from?

       

      Marty