8 Replies Latest reply on Nov 8, 2019 11:31 AM by shabaz

    Lag when using 7" touch screen.

    fischermachine

      Hi there,

       

      I'm experiencing constant lag on loading screens and in all games in a rhythmic pattern in conjunction with the sound. I have multiple Pies and SD card builds that all work perfectly with HDMI tvs and monitors, but all have the same lag issue with this screen. I've updated all core packages from the retropie setup script. Between loading screens I get this error: 1V10 volume control :: init() - failed to find mixer elements.

       

      Here is my setup:

       

      Retropie on a PI 3 B+

      Element 14 Raspberry Pi 7" Touch Screen Display

      Northpada 5V 3A power supply

       

      Not sure what else to do,
      Will