2 Replies Latest reply on May 9, 2020 4:01 AM by dpechkin

    UltraZed-EV starter kit kernel boot problem.

    dpechkin

      Hello!

       

      I have the UltraZed-EV System-on-Module Starter Kit.

      I have the petalinux-2019.1 and UltraZed-EV Carrier Card—PetaLinux 2019.1 Enhanced BSP.

       

      I created a project and checked that the root file system type is initramfs.

      And It was built successfully after these steps.

       

      I set a switch to jtag mode (On-On-On-On) and upload u-boot via command: petalinux-boot --jtab --u-boot.

       

      I set the server IP of the TFTP server and executed the command "run netboot" in the u-boot console.

      The image is uploaded, and the kernel was started.

       

      The kernel was hanged on after these lines:

      console [ttyPS0] enabled at MMIO 0xff000000 (irq = 46, base_baud = 6249999) is a xuartps

      [    3.535829] console [ttyPS0] enabled

      [    3.539420] bootconsole [cdns0] disabled

      [    3.539420] bootconsole [cdns0] disabled

      [    3.547328] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 47, base_baud = 6249999) is a xuartps

       

      The full console log is attached.

       

      I have the same issue for the project for the SD card.

      The switch was set to OFF-ON-OFF-ON for that rootfs type.

       

      Maybe I missed some steps?

      Anyone can give some advice?

      Thanks in advance.