0 Replies Latest reply on Jun 3, 2021 9:41 AM by dagnolof

    RaspBerry Pi 7 Inch Touchscreen Remote VNC desktop resolution

    dagnolof

      Hi,

       

      I bought a 7 inch touchscreen for raspberry Pi 3b+ and is working fine on Touchscreen resolution 800 x 480 pixels.

       

      When i connect a remote desktop via VNC it also takes the resolution 800x840 pixels iso 1920x1080

      Witch is making the icons far to big.

       

      When i disconnect 7-inch touchscreen, remote VNC desktop resolution switches to 1920x1080 without changing the

      settings.

       

      Is it possible to force VNC connections to 1920x1080 resolutions togheter  with 7-inch touschreen connected.

       

      /Boot

      config.txt

       

      I have set

       

      hdmi_force_hotplug=1

       

      # uncomment to force a specific HDMI mode (this will force VGA)

      hdmi_group=2

      hdmi_mode=82

      hdmi_ignore_edid=0x5000080

       

      Thanks in advance for any advice on this issue

       

      Best regards,

      Fabrizio