0 Replies Latest reply on Jul 21, 2021 11:15 AM by malakai00

    Wi-Fi not working on Portenta H7 M4 Core?

    malakai00

      I have a very simple sketch that runs on the M7, it simply boots the M4 core and then in the loop blinks the Red LED.

      I have a sketch loaded to the M4 core to create an Access Point and perform some other work. When the M4 boots up I see a messages on Serial1 indicating it is attempting to create an access point using WiFi.beginAP. That call never returns so it is blocking on something.

      The same Wi-Fi sketch works as expected on the M7 core.

      Has anyone used Wi-Fi on the M4 core?