Skip navigation
>

Lec 3 - Developing Application for Blinking LED with Interrupt (part 1)

Description:

Download these Lectures Resource Files from Github: https://github.com/uElectron/minizedSDK ====================================================================== In this Video , using the Minized Board based on Xilinx Zynq : 1.)We Develop Application which Blinks PS LED controlled with PS Button by using Interrupts instead of Polling and We create a Changing Pattern in LED Blinking 2.)We Develop PL LED Blinking Application by using the GPIO driver in PL based on the Hardware Design 3.)We can see how to use Example Programs to develop our own Interrupt Based Applications.

This video is embedded in the following content:
Developing Interrupt Based LED Blinking Application on Zynq - Minized Board

Comments