Skip navigation
>

NOVSIS - an NFC-based Office Visitor Sign-In System (POC Demo)

Description:

This is a working demo of NOVSIS, which is an NFC-based Office Visitor Sign-In System.

 

The system uses a PN7150 NFC controller in multiple modes. It reads NDEF data from NFC Tags, to provision WIFI, for example. It uses P2P mode to exchange information to the cellular/mobile smart phone so that it can connect via Bluetooth LE, and it writes byte data to MIFARE cards.

 

As part of the working demo I have a RC522 connected to a MKR1000 MCU, which will eventually be used to connect to the cloud for access control. Here the RC522 is used to read the data of a MIFARE card and confirm via Serial Monitor the PN7150 MIFARE card write.

 

My blog write up as part 2 of my Project14 NFC project submission to follow shortly.

This video is embedded in the following content:
NOVSIS: the NFC-based Office Visitor Sign-In System – PART 2 (Unpacking the POC demo)

Comments