Bengaluru,
15
August
2024
|
06:05
Europe/Amsterdam

element14 Enables Base Stations to Increase 5G Capacity with New Toshiba Antenna Switch

With the rollout of 5G continuing at pace, new Toshiba device improves RF switching in compact package

Image_release

element14 is now shipping the new high-power SPDT (Single-Pole Double-Throw) RF antenna switch from Toshiba.

The SPDT RF (TCWA1225G) switch is important for the expansion of 5G networks. This is because the expansion requires antennae that are increasingly composed of complex signal transmission paths that need RF switching with low insertion loss and high input power, but in a compact package.

In response, the SPDT RF offers an input peak power of 46 dBm (at 8dB PAR) in a very small footprint. This means that while antenna size can be maintained, or even reduced, power output can remain consistent.

Toshiba’s SPDT RF switch was designed and produced in response to the increased introductions of massive MIMO (Multiple Input, Multiple Output) technology in telecommunications base stations, which use multiple transmit and receive antennae to provide ultra-high speed and ultra-large capacity radio communications services essential for 5G.

Individual antenna are also increasingly composed of super-multi-element antennae and complex signal transmission paths. Traditionally, RF switching is generally used for switching between complex transmission paths. However, the RF switch must have low insertion loss, high input power and be small enough so that the number of RF switches and the size of antennae would not increase due to space limitations. The SPDT RF switch resolves both of those limitations.

Jose Lok, element14 Product Category Director, Semiconductors, said, “This switch is a major accelerator for 5G and it’s essential that it’s widely and readily available to fulfil the promise of 5G networks. We are delighted to work with Toshiba to ensure this space and cost-saving device delivers its full potential in ensuring 5G implementation.”

The SPDT RF switch from Toshiba is now available and shipping from Farnell in EMEA, Newark in North America and element14 in APAC.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com/