Farnell now stocking Omega’s HANI™ Clamp-on Temperature Sensor
The award-winning Omega engineering clamp-on temperature sensor is the first of its kind to offer highly accurate measurement of fluid inside a pipe without having to insert a probe.

Farnell, an Avnet Company and global distributor of electronic components, products and solutions, is now stocking the latest innovation for non-invasive temperature measurement, the HANI™ Clamp-on Temperature Sensor from Omega Engineering.
The HANI is available from Farnell and offers customers the unique ability to measure the temperature of fluid inside a pipe without having to install an invasive sensor. Offering unprecedented accuracy when taking temperature measurements of sanitary fluid and industrial processes, it is an ideal solution for food and beverage, personal care, chemical production and pharmaceutical applications.
The award-winning HANI Clamp-on Temperature Sensor can be installed in seconds on metal pipe sizes 1”- 4” and incorporates temperature and heat flux sensors with a proprietary algorithm to deliver fast measurements, reducing downtime and installation costs. With a response time of 5 sec (t63) and 10 sec (t90) measurements, the HANI offers high accuracy in metal pipes, achieving ±0.5°C in sanitary applications and ±0.5 to ±1.0°C in industrial installations.
As a Layer N-compatible device, the HANI can be seamlessly connected within Omega’s smart industrial monitoring and control ecosystem. The HANI outputs at 4-20 mA and can be connected by an M12 cable to any standard output device.
Mike King, Global Product Segment Leader - Sensors at Farnell said: “Omega Engineering is a market leader in the development of innovative industrial control and measurement products, and the HANI™ Clamp-on Temperature Sensor is no exception. We are pleased to bring Omega’s full portfolio of advanced technology products to our customers.
“The HANI is a truly unique solution as it can be mounted like a surface sensor in seconds, but it offers the performance of an invasive sensor. Customers don’t have to worry about immersion depth, material compatibility, corrosion or contamination risks, and will benefit from reduced costs and maximised uptime when measuring fluids used in critical processes.”
The HANI™ temperature sensor mounts like a surface sensor, but performs like an invasive sensor. Installing or relocating an invasive in-pipe sensor can be a costly, time-consuming process. With the HANI, customers don't need to worry about immersion depth, material compatibility, corrosion or contamination risks. And there's no loss of performance, so it's really a best-of-both-worlds approach”, said Ahmar Bajwa, Director Product Management, Temperature Products, Omega Engineering.
Omega Engineering, part of Spectris Plc, is an established manufacturer of innovative solutions, offering more than 100,000 state-of-the art products for the measurement and control of temperature, humidity, pressure, strain, force, flow, level, pH and conductivity. Omega also provides customers with a complete line of data acquisition, electric heating, and custom engineered products.
The HANI Clamp-on Temperature Sensor from Omega Engineering is now available for fast delivery from Farnell in EMEA, element14 in APAC and Newark in North America.
About us
Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Farnell trades as Farnell in Europe, Newark in North America, and element14 throughout Asia Pacific. Farnell's global businesses are supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Farnell also sells direct to consumers through a network of resellers, and its CPC business in the UK.
Farnell is a business unit of Avnet (Nasdaq: AVT). Avnet is a global technology solutions provider with an extensive ecosystem that delivers design, product, marketing and supply chain expertise for customers at every stage of the lifecycle.
For more information, visit the website at http://www.farnell.com/corporate