Farnell signs new distribution agreement with KUNBUS
The devices, gateways and expansion modules from KUNBUS can save designer engineers time and money when developing new industrial automation and control applications.
Farnell, an Avnet Company and global distributor of electronic components, products and solutions has signed a new distribution agreement with KUNBUS to further enhance its portfolio of solutions for industrial automation and control applications. Design engineers can save time and money when using the devices, gateways, and expansion modules in the KUNBUS portfolio to implement Industry 4.0 into their business.
KUNBUS specialises in industrial communication for automation, process, manufacturing and drive technology provided by its modular open-source Raspberry Pi-based hardware platform, Revolution Pi. This flexible and cost-effective industrial-grade device delivers the performance and simplicity of the Raspberry Pi to the industrial control market. Farnell customers now have a broader range of solutions when designing automation and Industrial Internet of Things (IIoT) projects. The extra functionality offered by the digital and analogue expansion modules and gateways from KUNBUS also facilitate retrofitting.
The portfolio of products from KUNBUS are now available for fast delivery from Farnell, including:
· RevPi Connect+: Powered by Raspberry Pi Compute Module 3+, the device offers users maximum freedom when designing and implementing IIoT projects due to the open platform concept. Two Ethernet sockets enable the device to be simultaneously connected to the automation network and IT network, allowing it to transmit machine data from the shop floor to the cloud or a higher-level IT system. RevPi Connect also features two USB sockets, one micro-HDMI socket and one micro-USB socket.
· RevPi Core 3+: With up to 32GB flash memory, the RevPi Core 3+ is an ideal base module for those requiring more storage space than offered by its predecessor the RevPi Core 3. Powered by the Raspberry Pi Compute Module 3+, the RevPi Core 3+ has two USB sockets, a HDMI socket, a micro-USB socket and an Ethernet connection as interfaces.
· Digital and Analog I/O Modules: The range of digital and analog modules can transform Revolution Pi into an industrial control unit when connected to the base module RevPi Core. Three versions are available: a standard version with 14 digital inputs and 14 digital outputs, and two special versions that have either 16 digital inputs or 16 digital outputs. All are fitted with the same 28-pin I/O connector at the front. The RevPi Analog I/O (AIO) expansion module adds four analogue inputs, two analogue outputs and two RTD channels to a Revolution Pi system. Inputs, outputs and RTD channels are galvanically isolated to each other and to the logic circuit. RevPi AIO is protected against interference according to EN 61131-2 requirements and may be operated from -30 °C to+ 55 °C ambient temperature.
· Modular Gateway Solution Series: Enabling continuous and reliable communication between different networks and systems, the Modular Gateway Solution Series from KUNBUS effectively converts all data that a target network can transfer. It omits non-transferrable data and adds necessary data in the new network to ensure communication from one closed network to another. Compact plug-and-play DIN-Rail mounted protocol converters may be added to connect one network to another and are simple to exchange as required.
Romain Soreau, Head of Single Board Computing at Farnell, said: “We are delighted to add KUNBUS to our portfolio. They are a significant addition to our ever growing offering of SBC solutions for industrial automation and control applications. KUNBUS offers a platform that further extends the performance and simplicity of the Raspberry Pi to industrial environments with the added benefit of enabling our customers to retrofit to existing systems which is a challenge in most sectors.”
As a global distributor, Farnell provides customers with fast access to easy-to-use products for professional use with a broad range of core SBC platforms and toolkits from leading brands including Raspberry Pi, Intel (NUC range), Industrial Shields and more. Technical support is offered 24/5 to ensure engineers can take advantage of the latest technology innovations for experiments and new product design.
Farnell can support customers as they take ideas from specification through to production with end-to-end product development solutions offered via the Avnet ecosystem. Customers also benefit from free access to valuable online resources on the Farnell website, and engineering and maker community, element14.
A range of devices, gateways and expansion modules from KUNBUS are now available from Farnell and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com