Premier Farnell adds new FLIR ETS320 to its Test & Measurement Portfolio
New FLIR camera provides hands-free, sensitive thermal imaging for electronics testing in the Laboratory

Premier Farnell, the Development Distributor, is now shipping the new FLIR ETS320 Thermal Imaging camera, designed for quick temperature checks on printed circuit boards and other small electronics in the laboratory and accurate quality assurance and factory acceptance testing.
Heat can be an important factor in understanding how a system is functioning and the FLIR ETS320 provides non-contact thermal measurement through a combination of a high sensitively infrared camera with an integrated stand for hands free measurement.
The new camera delivers significant benefits for users:
-
Reduced test times: The camera can quickly identify hot spots, thermal gradients, and potential points of failure, detecting temperature shifts as small as (<0.06c) and quantifying heat generation up to 250oC.
-
Improved product design: The camera has 78,000 points of non-contact measurement enabling users to identify where and when to add fans and heat syncs to ensure products operate within specified parameters for maximum lifetime. A temperature measurement accuracy of ±3°C makes the camera ideal for quality assurance and factory acceptance testing.
-
Optimize lab time: The camera is designed for hands-free use in the lab with a micro-scope style stand that is easy to set up and suited to testing small electronics. The camera is battery operating removing the inconvenience of wires and has simplified features offering complete measurement and analysis on the camera, alongside ease of use.
-
Save money: Improves rapid prototyping and reduces product development cycles.
Key features include a 320 x 240 pixel IR detector non non-contact measurement, crisp 3” LCD display providing immediate thermal feedback, 45° field of view, thermal sensitivity (NEtD) of 0.06°C, temperature measurement accuracy of ±3°C and a wide temperature range of up to 250°C, and hands free-battery operated measurement.
The new FLIR camera is available to buy from Farnell element14 in Europe, as well as Newark element14 in North America and element14 in Asia Pacific.
About us
Premier Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Premier Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Premier Farnell is a business unit of Avnet, Inc., (NYSE:AVT). Premier Farnell trades as Farnell element14 in Europe, Newark element14 in North America, and element14 throughout Asia Pacific. The Premier Farnell Group is supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere.
For more information, visit the website at http://www.premierfarnell.com