WaRP7 provides greater flexibility and rapid development for IoT and wearables applications
WaRP7 IoT and wearable development platform now available exclusively from element14

Set to be a game changer for the Internet of Things (IoT) and wearables market, the WaRP7 development platform enhanced by NXP® Semiconductors, designed and manufactured in partnership with element14 is now available to buy. Built from the ground up to address key challenges for design engineers such as size, battery life and connectivity, the open source design and complete software package of WaRP7 allows developers to innovate without licensing restrictions, reducing time to market and moving focus to product differentiation in this rapidly growing market. The continual focus on smaller, lighter and more powerful components has expanded this market creating new opportunities for design engineers.
The rapidly growing IoT market presents new challenges and is forcing a change in the industry, pushing design and manufacturing into unchartered territory. WaRP7 is built to meet the needs of a broad range of applications including smart home, sports and heart rate monitors and wearables.
Our experience in small form factor design, manufacturing capability and experience in supporting the development community has helped create the WaRP7, a device that we believe addresses today’s most pressing technology challenges and provides the longevity of design to remain relevant as the market continues to develop. We believe this is a game-changing device and will potentially help answer the question of what is needed to be successful in the wearables market.
Features include:
- Battery Life: WaRP7 is based on the NXP i.MX 7Solo applications processor. The unique heterogeneous multicore architecture enables low-power modes critical for most IoT and wearable designs, but also provides the power to drive a higher-level operating system and a rich user interface.
Connectivity: WaRP7 offers a variety of connectivity options enabling a wide range of usage models including near-field communications. The Murata®-type 1DX multi-radio module offers 802.11b/g/n + Bluetooth 4.1, classic and low energy.
Usability: WaRP7 is flexible enough to offer all the advantages of traditional development tools and is free of licensing restrictions due to its open-source design.
Miniaturization: WaRP7 is one of the smallest development system with the size of its main CPU board of approximately 2 x 4 centimetres.
WaRP7 is one of the most power-efficient processor based development platforms for evaluation and rapid adoption into original small form-factor product designs on the market. By utilizing the heterogeneous multicore architecture of the i.MX 7Solo device, WaRP7 allows customers to optimize power efficiency, lower the bill of materials, and benefit from the ultimate in performance flexibility to address the varied usage models for the IoT and wearables market.
WaRP7 is based on the NXP i.MX 7Solo applications processor that features an advanced implementation of the ARM® Cortex®-A7 core, as well as the ARM® Cortex®-M4 core. It comes with features such as on-board sensors, connectivity including NFC, Bluetooth®, Bluetooth Smart and Wi-Fi®, and on-board external LPDDR3 memory. WaRP7 offers rich multimedia capability with access to MIPI-DSI display port, on-board camera and audio features. It is highly integrated with on-board sensors, rechargeable battery and power circuitry.
WaRP7 eases development effort for software developers with access to Linux and supports extensive UI capabilities and connectivity stacks. WaRP7 is truly expandable with the MikroBus™ expansion socket opening users to over 200 compatible Click Boards™.
WaRP7 is backed by the development community, design and manufacturing capabilities of element14 and is available from element14. For more information, visit www.element14.com/WaRP7.
About the Premier Farnell Group
Premier Farnell plc (LSE:pfl) is a global leader in high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Trading as Farnell element14 in Europe, Newark element14 in North America and element14 across Asia Pacific, it had sales last year of £982.7m, the Group is supported by a global supply chain of more than 3,000 suppliers and an inventory profile developed to anticipate and meet its customers’ needs.
Premier Farnell works to bring to market development kits in a variety of applications, enabling it to support the customer from design concept through to production.
The latest products, software, services and solutions from trusted supplier partners are all available through 43 local language transactional websites. The element14 Community allows buyers and engineers to access a wide range of independent technical information, tools and the latest resources and the Design Center enables design engineers to compare kits from the world’s greatest range of development tools.
For news updates from Premier Farnell and element14 visit:
Premier Farnell News Centre – www.premierfarnell.com/media-centre
Twitter - @element14
YouTube – element14
Facebook – facebook.com/element14page
Email: pressoffice@premierfarnell.com
Premier Farnell Key facts
- Operations in 38 different countries
- More than 4,500 employees
- More than 3,000 leading suppliers
- More than 600,000 products stocked with access to over four million more on demand
- Leaders in providing information on REACH, Conflict Mineralsand EU RoHS legislation
For more information visit the website at Premier Farnell.