Leeds,
28
July
2020
|
09:30
Europe/Amsterdam

Complete range of Omega sensing and process control products now available from Farnell

Farnell now stocks Omega’s full range of state-of-the-art temperature, pressure, flow and level sensors, as well as transducers, automation and control products, and connectors.

FAR 516 - inline image

Farnell, the Development Distributor, has dramatically enhanced its industrial automation and control portfolio with a greatly expanded range of products from Omega. This new agreement makes Farnell the only high-service distributor selling Omega products in Europe. Electronic design, industrial and maintenance engineers can now buy Omega’s world-class range of products for measurement and control of temperature, humidity, pressure, strain, force, flow, level, pH and conductivity from Farnell.

Omega helps customers in aerospace, automotive, wireless, test and measurement, process control and power monitoring to connect their systems. The Omega range of sensing, heating, automation, data acquisition and control solutions now available from Farnell includes:

  • CN16PT-330 PID Controller: The powerful and versatile Platinum Series family of microprocessor-based PID controllers offers unparalleled flexibility in process measurement while being easy to setup and use. Their universal inputs support thermocouples, RTDs, thermistors, process voltage/current and strain, sampling data at up to 20 samples per second with a 24-Bit ADC. Connectivity is via standard USB, optional Ethernet and RS232/ RS485 with Modbus® Serial Communications. They are especially suited to applications where visual verification is important, such as factory automation, mechanical testing and process industries (including food, plastics and ceramics processing) as well as laboratories.
  • NOMAD OM-91 Temperature Data Logger: The portable, battery-powered data logger is compact, lightweight and easy to use for accurate and repeatable logging of temperature. The graphical user interface for configuring new devices and collecting data is intuitive, and it features LED status indicators and a USB interface for fast data transfer. This temperature logger excels in transportation applications where it is necessary to document that a material in-transit has remained within environmental limits and may be used in multiple data logger installations.
  • OS136A-1-K Infrared Temperature Sensor/Transmitter: This miniature, low-cost, non-contact and high-performance combined infrared temperature sensor and transmitter is supplied with a 1.8m shielded cable for power and output connections. It is available with two measurement ranges of -18 to 202°C and 149 to 538°C. Industry standard outputs provide easy interfacing with all meters, controllers, data loggers, recorders, computer boards and PLCs. Applications include measuring temperature in hard to-reach, confined or harsh environments.
  • FL-500 Series In-line Flowmeters: Featuring rugged construction and easy installation, the FL-500 Flowmeters offer direct-reading flow rates for water and air at atmospheric and 6.2 bar (90 psi) pressures. Settings are easily adjustable with a screwdriver and proximity switches can be added to signal specific flow rates. FL-500 Flowmeters can be used for flow rate indication for liquids, gases and steam.

Simon Meadmore, Global Head of IP&E at Farnell says: “We are delighted to provide an expanded range of specialist industrial automation and process control products from Omega through this new agreement in Europe. We now offer our customers fast delivery of the largest range of Omega products available from a single source. Great quality and high reliability make Omega the first choice for our customers building industrial control applications.”

Omega has been in business for more than 55 years and is a respected market leader. Farnell’s customers have access to a very wide range of market leading automation and control products with 24/5 technical support. This includes free online resources, data sheets, application notes, videos, and webinars on Farnell’s website.

Omega’s range of sensing and process control products are available for fast shipping from Farnell in EMEA and element14 in APAC.

Boilerplate

About us

Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.

Farnell trades as Farnell in Europe, Newark in North America, and element14 throughout Asia Pacific. Farnell's global businesses are supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Farnell also sells direct to consumers through a network of resellers, and its CPC business in the UK.

Farnell is a business unit of Avnet (Nasdaq: AVT). Avnet is a global technology solutions provider with an extensive ecosystem that delivers design, product, marketing and supply chain expertise for customers at every stage of the lifecycle.

For more information, visit the website at http://www.farnell.com/corporate