London,
23
January
2017
|
11:01
Europe/Amsterdam

element14 exclusively launches BitScope Blade for Raspberry Pi

A robust power and mounting solution for the industrial deployment of Raspberry Pi

BitScope Blade Uno, Duo, Quattro.jpg

element14, the development distributor, today announces exclusive global availability of the new BitScope Blade range, offering the ability to conveniently power and mount multiple Raspberry Pi’s.

BitScope Blades are designed for building scalable computing solutions ranging from stand-alone servers, routers and workstations up to full compute clusters, private clouds, networked physical computing and Industrial IoT systems.

Every Blade can be used with simple plug packs, 12V batteries, solar power systems, low cost uninterruptible power supplies (UPS) and even passive power over Ethernet (PoE) solutions to up 48V. They may be used individually on the desktop, wall mounted or multiple Blades may be installed in racks for large scale deployment. Blades offer full access to Raspberry Pi I/O for displays, cameras, keyboards, expansion boards and peripherals including BitScopes, Raspberry Pi HATs and the Raspberry Pi 7” Touchscreen Display.

BitScope Blade is available in three editions based upon the number of Raspberry Pi boards mounted:

  • BitScope Blade Uno is a flexible power and mounting solution for one Raspberry Pi computer and optional HAT. It is the perfect computing platform for makers, students and engineers using the Raspberry Pi.
  • BitScope Blade Duo is a desktop, rack or wall mountable power and mounting solution for a pair of Raspberry Pi computers, ideal for building a reliable stand-alone desktop & server system with the Raspberry Pi.
  • BitScope Blade Quattro is a desktop, rack or wall mountable power and mounting solution for four Raspberry Pi computers, ideal for creating compute clusters, private clouds or build farms with the Raspberry Pi.

Claire Doyle, Global Head of Raspberry Pi and Single Board Computing for element14, said: “The BitScope Blade is a really exciting addition to our ecosystem of Raspberry Pi accessories as it increases potential to use the Raspberry Pi within new applications as well as providing power reliability required for industrial use. We work with an increasing number of start-ups designing-in the Raspberry Pi for commercial and industrial use. This new product has the potential to create a step-change in opportunities within the industrial sector, and facilitate a revolution in the use of single board computers within industry”

Bruce Tulloch, CEO of BitScope Designs, said: “Our experience working with hundreds industrial customers using BitScope with Raspberry Pi demonstrated the key problem most of them faced was finding a cost effective, reliable and scalable power and mounting solution for Raspberry Pi and its accessories. BitScope Blade is our solution, customised specifically to the needs of our industrial, commercial and educational customers.”

The product is expected to appeal to professional engineers, students and hobbyists as a solution to broaden industrial design applications for Raspberry Pi.

The BitScope Blade products are available from Farnell element14 in Europe, Newark element14 in North America and element14 in Asia Pacific. For more information on the BitScope Blade range please visit the element14 community.

Download Media Kit
Download
Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,300 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com