Leeds,
27
April
2015
|
00:00
Europe/Amsterdam

element14 is First to Stock Two New High-Performance KEMET Capacitors

element14 has announced it is now stocking two new high-performance metalized impregnated paper series film capacitors from KEMET: the P278, Class X1, 480 VAC and the P295, Class Y1, 500 VAC.

Used primarily for electronic design engineers, these paper capacitors are the best EMI capacitors in terms of safety, reliability, overvoltage and transient handling, self-healing capability and long-term connection to the mains. They have high resistance to ionization and are more stable than any other dielectric available on the market.

The new capacitors are ideal for industrial use with pumps circulators or special high-reliability power supplies. They’re constructed of multilayer metalized paper encapsulated and impregnated in self-extinguishing material meeting the requirements of UL 94 V-0.

Typical applications for the P278 Series include worldwide use as an electromagnetic interference suppressor in all X1 and across-the-line applications. Typical applications for the P295 Series include safety capacitors for bridging of double or reinforced insulation applications requiring voltage test up to 4,000 VAC at 60 seconds. P295 Series capacitors can be left in place during this test.

Priced as low as $.58 and available with next day delivery, the KEMET P278, Class X1, 480 VAC and P295, Class Y1, 500 VAC high-performance metalized impregnated paper series film capacitors are available from Newark element14 in North America, Farnell element14 in Europe and element14 in APAC.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com