Bengaluru,
24
April
2025
|
05:31
Europe/Amsterdam

element14 adds innovative NXP® Semiconductors microcontrollers and FRDM development boards to portfolio

New MCX series microcontrollers deliver innovation to do more with expanded MCU capabilities and enriched development platform

NXP img1

element14 has announced the addition of NXP® Semiconductors’ all-purpose MCX-series of industrial and IoT microcontrollers to its portfolio; plus new FRDM development boards in a platform that removes limitations to a design engineer’s imagination.

The MCX A series includes the MCX A13x, MCX A14x, and MCX A15x. These are mainstream, easy-to-use MCUs with an innovative power architecture and software compatibility necessary for embedded applications, such as industrial sensors, motor controls, battery or handheld power system controllers, IoT devices and more.

Powered by the Arm® Cortex®-M33, the MCX A series are general-purpose MCUs designed to address a wide range of applications with scalable device options, low power and intelligent peripherals. The innovative power architecture is designed to support high I/O utilization and power efficiency with a simple supply circuit in a small footprint.

The MCX C series MCUs are powered by Arm Cortex-M0+ up to 48 MHz and are designed for energy efficiency and cost effectiveness, making them well-suited for a wide variety of applications. Featuring USB and segment LCD options, these MCUs cater to diverse needs, providing flexible and scalable memory and packages.

MCX N series of highly integrated Arm Cortex-M33 microcontrollers are designed for high performance and low power consumption. MCX N includes intelligent peripherals and on-chip accelerators providing multitasking capabilities and performance efficiency. Select MCX N families include NXP's eIQ® Neutron neural processing unit (NPU) for machine learning applications.

Finally, the MCX W series are secure, wireless MCUs designed for more compact, scalable and innovative designs for the next generation of smart and secure connected devices. The MCX W series, based on the Arm Cortex-M33, offers a unified range of pin-compatible multiprotocol wireless MCUs for Matter™, Thread®, Bluetooth® Low Energy and Zigbee®. MCX W enables interoperable and innovative smart home devices, building automation sensors and controls and smart energy products.

Justin Mortimer, NXP MCU Global Product Marketing Manager said: ““The NXP MCX portfolio is foundational for the future of power-efficient edge devices across industrial and IoT markets. The new MCX MCUs use the improved MCX + FRDM platform to integrate essential features that give engineers the freedom to design without limitation.”

The MCX series is accompanied by NXP’s newly enhanced FRDM development boards, a low-cost, scalable hardware platform supported by the MCUXpresso Developer Experience toolset. Designed to encourage creative freedom, these compact boards promote flexible and rapid prototyping, with industry-standard headers providing easy access to the MCU’s I/Os. With the on-board MCU-Link debug probe and USB-C cable included, engineers can develop, program and debug with ease.

  • Comprehensive Software Enablement

The FRDM boards and MCX portfolio are supported by the widely adopted MCUXpresso ecosystem of software and tools to provide an optimal developer experience. Developers can work with either MCUXpresso for Visual Studio Code, the Eclipse-based MCUXpresso IDE from NXP, or with IDEs from IAR and Keil that also offer safety certification. NXP provides drivers and middleware with examples ready to work out of the box for any of these IDE choices, along with additional tools for device configuration, security and specialist applications.

Jose Lok, Global Product Category Director, Passives and Semiconductors at element14, said: “We are thrilled to announce the addition of the NXP MCX microcontrollers to our offerings. The microcontrollers have been designed to cater to a broad range of edge applications and will become a popular choice among design engineers due to its focus on scalability. These additions reflect our commitment to empowering our customers and partners to succeed in the ever-evolving technological landscape.”

The MCX series and enhanced FRDM boards can be ordered online from Farnell in EMEA, Newark in North America and element14 in APAC.

 

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com