element14 now stocking LattePanda Mu
Latest addition to the popular LattePanda range proves popular
element14 has announced that LattePanda Mu compute module, carrier boards, and starter kit, the latest additions to the popular LattePanda range from DF Robot, are now available from stock.
LattePanda Mu is a micro x86 compute module that features an Intel N100 quad-core processor with 3.4GHz turbo frequency. This combination provides solid performance and multitasking capabilities for the majority of applications. Small, yet powerful, LattePanda Mu supports multiple operating systems, including Windows 10, Windows 11, Linux, and others with a wide range of flexible customisation options.
Its small, pocket-size dimensions enable the LattePanda Mu x86 compute module to be easily integrated into space-constrained devices, delivering powerful computation without taking up much space.
Romain Soreau, Global Program Manager, Single Board Computing at element14, said, ”LattePanda Mu builds on the success of LattePanda - a complete single board computer that can do everything a regular PC can do including running powerful tools such as Visual Studio, NodeJS, Java, Processing, and much more. Its compute module, carrier boards, and starter kit comprise an attractive package of speed, power and flexibility.”
LattePanda Mu enables users to freely allocate the interfaces and form factors they need in the carrier board design, whether it be for an energy-saving or a high-performance, 10GbE network equipped, NAS.
The processing and encryption/decryption performance of the N100 processor included in the LattePanda Mu enables multiple network cards to be used to achieve the network functions required. Further functions can be added to the carrier board to build it into a highly integrated and versatile network infrastructure.
Joy Yang, Business Development Manager for DFRobot, said “The LattePanda Mu’s flexible ports and open-source carrier board files enable users to effortlessly design custom carrier boards to meet their unique requirements. It has been a very popular addition for DFRobot and will no doubt be equally successful with element14’s customers.”
The LattePanda Mu is now available and shipping globally from Farnell in EMEA, Newark in North America and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com