Bengaluru,
10
October
2024
|
10:42
Europe/Amsterdam

element14 now stocking Abracon's new AOTA series mini-moulded inductors

New inductors offer same performance advantages as their larger counterparts

Abracon-AOTA

element14 has announced the availability of Abracon's new AOTA Series mini-moulded inductors.

Building upon the success and advantages of its traditional moulded inductors, Abracon has expanded its moulded inductor technology into the realm of sub-3mm inductors which, despite their compact size, deliver the same exceptional performance as their larger counterparts.

element14 Supplier Account Manager and Abracon specialist, Euan Gilligan, said: “The mini-moulded inductors deliver all the benefits of traditional moulded inductors, including superior EMI shielding, high power density, and low core losses, despite their small size. The benefit is that these inductors effectively mitigate unwanted EMI, handle significant power loads, and exhibit low core losses, thereby ensuring enhanced signal integrity, space efficiency, and improved energy efficiency in electronic circuits.”

By migrating the power of its moulded inductor technology to smaller package sizes, Abracon continues to provide solutions that meet the evolving needs of the electronics industry.

For example, Abracon's AOTA Series is highly suited to IoT, machine-to-machine, secure car access, item tracking, indoor navigation and other connected applications. They are an ideal alternative to traditional resin-shielded or multi-layer inductors, offering higher performance at a lower cost in a smaller size.

The AOTA Series inductors are available from element14 in 1.4mm x 1.2mm to 2.5mm x 2.0mm package sizes with a maximum height as low as 0.65mm to support small and low-profile designs.

They are available with inductance values from .11 to 10 µH with low DCR, low core losses and saturation current up to 14.5 amps to support significant power loads and high-power density requirements.

 All Abracon AOTA Series inductors are available and shipping from Farnell in EMEA, Newark in North America and element14 in APAC.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com