Farnell Adds Ikalogic to Test and Measurement Range - Featuring the World’s First Wireless Oscilloscope Probe
Test instruments and software for creative electronics and firmware engineers
Farnell, the Development Distributor, has added Ikalogic to its test and measurement range, extending its portfolio of competitively priced logic analysers and handheld oscilloscopes. Designed with engineers in mind, Ikalogic products will be welcomed by electronic design and firmware engineers, embedded designers and makers, enabling them to capture and analyse signals with ease.
Offering a high degree of flexibility in use, Ikalogic’s product range includes both wireless and battery operation (enabling isolation from mains voltage) and software which runs on Windows, macOS and Linux operating systems. The standard USB connection turns any computer into a measuring system allowing processing of hours of high frequency signals and identification of rare events. State of the art hardware guarantees reliable measurements and open-source add-on scripts offer in-depth analysis.
Key products available for same day despatch from Farnell include:
- IkaScope WS200 is a revolutionary, ultra-portable, battery powered wireless oscilloscope probe, the first of its kind anywhere in the world, making measurement and debugging simpler than ever before. The IkaScope connects to any WiFi enabled screen including desktop computer, tablet or smartphone to display captured signals and reliable measurements within a few seconds of using the product. Its patented ProbeClick® technology automatically holds captured signals when the probe tip is released.
- SP209 Series 9-Channel, 200MSPS logic analyser features an embedded 2 GB sampling memory and industrial bus receivers. The SP209 can capture logic signals and analyse I2C, SPI, CAN, RS232, 1-Wire, and 30 more protocols. The performance of the SP209 does not depend on USB connection bandwidth. The SP209 is ideal for embedded systems development and debugging, serial protocols analysis, industrial bus analysis, ADC (Analog to Digital Converter) diagnostics, reverse engineering, research and educational facilities.
- SQ series (ScanaQuad) is a low budget logic analyser which can capture, analyse and generate logic signals on 4 channels, at sampling rates up to 200MHz, allowing analysis and debugging of all serial protocols. Free ScanaStudio software is included to display, decode and analyse captured signals. Device performance does not depend on USB connection bandwidth. The SQ Series may be used for development and debugging of embedded systems and firmware, analysis of serial protocols, reverse engineering and education.
James McGregor, Global Head of Test and Tools for Farnell says: “We continue to offer our customers an ever-expanding range of competitively priced test and measurement products designed with engineers in mind. Farnell’s test and measurement range is all-inclusive and holistic, ensuring the engineering community is supported at every level, from beginners right through to professionals.”
Farnell offers its customers 24/5 technical support from their in-house test and measurement specialists and provides free access to online resources, data sheets, application notes, videos and webinars.
Ikalogic handheld oscilloscopes and logic analysers are available for same day despatch from Farnell in EMEA and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com