Leeds,
26
February
2019
|
09:30
Europe/Amsterdam

Premier Farnell Introduces Avnet SmartEdge IoT Gateway: A Low-Cost Device for Industrial Applications

Demonstrated at Embedded World Exhibition, Nuremberg, Germany, 26-28 February 2019

Inline

Premier Farnell, the Development Distributor, introduces the exclusive Avnet SmartEdge Industrial IoT Gateway; a new low-cost industrial gateway powered by Raspberry Pi. The Avnet SmartEdge Industrial Gateway will be showcased at Embedded World, Nuremberg, Germany from 26-28 February 2019 on stand 1-370.

The Avnet SmartEdge Industrial IoT Gateway enables seamless and secure connectivity to the cloud through Avnet’s IoT Connect platform running on Microsoft Azure, and is ideal for developing industrial automation applications such as, remote monitoring, predictive maintenance, process control and automation.

The gateway addresses key requirements for customers across a wide range of industrial applications – including additional ports to handle industrial protocols and a trusted computing module for added security on the hardware.

Connectivity options include a full set of industrial peripherals which include CAN-BUS and RS-232/ 485 (Modbus and DeviceNet) interfaces, isolated digital I/O and dual 10/100 Ethernet, with wireless connectivity including WiFi at 2.4 GHz and BLE 4.2 via an integrated antenna with external connectivity, plus an mPCIe interface for cellular modems. Power is via a 12-24 V DC input, and an HDMI display output is also incorporated. It is based on an 8 Gbyte EMMC which replaces the standard SD memory card, with security guaranteed by an onboard TPM 2.0.

The device also has the 40-pin expansion header to link with a range of devices from the ecosystem of HATs and other accessories.

The enclosure features space for an additional internal accessory to provide Zigbee, Z-Wave, or LoRa communications capabilities, for example, or for multiple accessories through case expansion. Mounting options include DIN rail, wall or free-standing.

“The Avnet SmartEdge Industrial IoT Gateway offers a level of simplicity, capability and accessibility never before achieved in this environment”, says Ralf Buehler, Senior Vice-President, Product Marketing & eCommerce, at Premier Farnell. “This new and exclusive product represents the value that Premier Farnell can add to customers as part of Avnet’s unique ecosystem, creating opportunities to develop new solutions for customers, based on strong existing relationships with the Raspberry Pi Foundation.”

Lou Lutostanski, VP, Internet of Things, Avnet adds “Developers familiar with prototyping on a Raspberry Pi device will find it a straightforward task to bring their designs to a production environment without ever having to switch platforms.”

Premier Farnell will demonstrate the Avnet SmartEdge IoT Gateway at Embedded World on stand 1-370 where it is co-located with its sister company, Avnet Silica. The demo will show a predictive maintenance application that features a range of industrial sensors mounted on a motor, that sends sensor readings to the Industrial IoT Gateway using common industrial protocols.

The Avnet SmartEdge Industrial IoT Gateway will be available from the summer from Farnell element14 in Europe and Newark element14 in North America.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com

Download