Leeds,
26
November
2015
|
00:00
Europe/Amsterdam

element14 first to stock Grid-EYE Sensor Evaluation Kit, powered by Panasonic allowing for fast prototyping

element14 has announced it is the first to stock the Grid-EYE Infrared (IR) Array Sensor Evaluation Kit, powered by Panasonic’s high-precision IR sensor platform for fast prototyping.

The Grid-EYE evaluation kit combines Panasonic’s industry leading Grid-EYE sensor, its “nanopower” PAN1740 Bluetooth Smart Module and a microcontroller on one PCB, enabling engineers to design and develop wireless sensor prototypes quickly. It can detect multiple people or objects moving in different directions; up, down, left, right and diagonally, including hand movements for gesture control.

The Grid-EYE Sensor Module includes an 8x8 IR pixel matrix, capable of measuring temperatures ten times per second over a wide temperature range (-20C to +100C). Communicating with the evaluation kit is achieved wirelessly using the built-in Bluetooth module or via a wired USB link.

The kit has two modes of operation; it can function as a standalone device or be connected to an Arduino DUE platform, for applications including motion detection, gesture control, detection of temperature distribution and Internet of Things.

Join the webinar on 3 Dec, 3pm GMT at http://www.element14.com/community/events/4485.

Additional features include bootloader accessible via a pin header, data display interface to PC and smartphone(Android and iphone) via USB or Bluetooth, reset switches for both board and Bluetooth, and Firmware/app loaded via JTAG header or USB port.

Priced from S$101.95 the Grid-EYE evaluation kit is available from element14 in Asia Pacific; more details at http://www.element14.com/community/docs/DOC-78673.
element14 is Panasonic’s number one high service distributor by product sales in Europe and boasts the manufacturer’s largest stocking profile in both Europe and Asia-Pacific. For more information on the product range visit http://sg.element14.com/panasonic-electronic-components.

 

 

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com