Leeds,
10
November
2021
|
06:00
Europe/Amsterdam

element14 Releases New Raspberry Pi Audio eBook

Presents new potential for Raspberry Pi in HD audio development without breaking the bank

FAR605 Inline Image

element14, an Avnet community, has released a new eBook for its members exploring the potential of Raspberry Pi for HD audio development and music creation. Audiophile makers typically rely on expensive systems to provide the best sound quality. With new add-on boards and fidelity software, Raspberry Pi is becoming a great option for HD audio enthusiasts.

Raspberry Pi is known for being a great tool for those learning to code and work with electronic hardware. New add-on boards are now available for the Pi 4 that offer top-of-the-line digital/analog converters (DACs) and amplifiers. Raspberry Pi has always had the hardware to produce high end audio and with these new HATs (hardware attached on top), the popular development board is now an excellent choice for audio editing and development on a budget.

Some of the new HATs highlighted in the eBook and available from Farnell to strengthen Raspberry Pi’s audio capabilities include:

  • JustBoom's JBM-001 DAC/Amp HAT: The board comes outfitted with a digital to analog converter (DAC) and a headphone amplifier that provides a 32-bit/384 kHz frequency. It also includes line-level RCA and headphone amplified 3.5mm jack outputs and volume control. It draws its power directly from Pi. The board also provides a 112dB signal to noise ratio (SNR) and -93dB total harmonic distortion (THD +N at -1dB). It can be used with the Raspberry Pi A+, B+, and 2B. Community members have used the JBM-001 to design multi-room audio players, media center stations, and stand-alone HD audio players.
  • Infineon's MERUS audio amplifier HAT: A great add-on board designed for the Raspberry Pi Zero, this HAT is great for sound amplification. The board is equipped with Infineon's MA12070P multi-level amplifier that provides up to 40 W of peak power. The add-on board draws its power from the Raspberry Pi and provides 24-bit/48 kHz audio playback. Complete hardware control, customization, and error monitoring are done via Linux Alsamixer. Its size allows users to task the amp with portable Pi projects, including players and speakers.
  • Micro Nova's AmpliPi multi-room/zone audio controller: The system is designed around a Raspberry Pi Compute Module 3+ and comes packed with PCM5102A and CM6206 audio DACs. The Pi can also communicate via I2C to an STM32F030 MCU integrated on a preamp board to control mixing and amplification systems. The AmpliPi is capable of streaming four independent sources to 6 stereo output zones, which can be expanded to up to 36 stereo output zones through daisy-chained extender units.

The eBook also highlights several software tools to make Raspberry Pi HD audio a reality. One of the better choices is the Sonic Pi. The live coding environment based in Ruby is versatile and allows users to create new sounds, work in a variety of musical styles, loop their audio, switch synths, and more. Other free software tools that work well with the Raspberry Pi platform include MilkyTracker and Tracktion Software’s Waveform DAW.

element14 is part of Farnell, an Avnet Company and global distributor of electronic components, which helps design engineers, maintenance and test engineers, makers, parents, and teachers develop the future generation of coders and products that apply technology to change our world for the better.

To read the full eBook and see all of the insights, please visit element14.com

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com