Leeds,
21
April
2021
|
09:50
Europe/Amsterdam

Farnell shares exclusive discounts and bundle deals for customers this spring

Customers can benefit from savings on market leading brands such as Tektronix, Omega, Omron, Schneider Electric and more.

Spring Campaign (1)

Farnell, an Avnet Company and global distributor of electronic components, products and solutions, is offering exclusive discounts to customers across Europe on a range of products from well-known brands including Tektronix, Omega, Omron, Rohde & Schwarz, Keysight, AMETEK and many more. Customers purchasing product bundles can also receive up to 50% off until 30 April 2021. The products included in the exclusive promotion will include components from Farnell’s passive, electromechanical, connector, development board, test, tool and production supply ranges, including:

  • VIRALERT 3 Human Body Temperature Screening System from AMETEK Land: This system uses thermal and visual cameras to provide temperature measurement and facial recognition whilst socially distanced. VIRALERT 3 scans a subject in approximately two seconds to enable seamless monitoring at a facility entrance, minimising delays and queues. This screening system from AMETEK Land is now available to Farnell customers with up to 25% off.
  • Advanced Power Applications Saver Bundle from Tektronix: This bundle of market leading test equipment from Tektronix is available exclusively to Farnell customers and includes an MDO34 Oscilloscope, Probes, 2231A-30-3 Power Supply, DMM6500 Digital Multimeter and KickStart Software. The Advanced Power Applications bundle represents a 20% saving compared to purchasing the products individually.
  • PM5000 Series Power Meters from Schneider Electric: A popular product from the PowerLogic range offering power quality analysis up to the 15th harmonic and flush-mounting. Farnell customers can purchase power meters in the PM5000 range with an exclusive 10% discount.
  • Solder Wire from Multicomp Pro: Specially formulated to complement no clean wave and reflow soldering processes, Multicomp Pro's lead-free 1.2mm diameter soldering wire is available exclusively from Farnell with a limited time 30% discount.

For more information and the full range of discounts available, visit Farnell’s spring offers page here.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com

Download Media Kit
Download