Latest products from TE Connectivity now available from element14
Fast delivery of the latest TE connectivity and sensor solutions accelerates new product development.

element14 has increased its TE Connectivity and sensor device portfolio with the introduction of their latest products, allowing customers to accelerate the development of new applications for electric vehicles, power, aircraft, digital factories, smart homes, life-saving medical care, efficient utility networks and global communications infrastructure.
These latest additions to element14’s existing portfolio of TE Connectivity products will aid new product development by providing customers with rapid access to a market-leading range of solutions from the world's leading manufacturer of innovative, reliable connectivity products and sensors.
The latest TE Connectivity additions to the element14 range include:
AMPMODU connectors are 2mm board-to-board receptacles that provide increased surface contact for reliable signal transfer and can be used in various mounting processes.
- Occupies 38% less space on PCB board compared with 2.54mm [0.1"] centreline.
- Two-point electrical stability for reliable header and receptacle interconnection.
- Multiple options for board-to-board stacking by headers and receptacles combination.
- Ease of assembly with automated surface-mount and through-hole reflow manufacturing.
- Applications include , servo drives, industrial controls, material handling, instrumentation, test equipment and building automation.
Corcom 3-phase high performance DIN Rail EMI filters are general purpose filters designed for use in 3-phase systems, with a neutral connection included.
- Designed to provide standard attenuation performance to reduce electromagnetic interference (EMI) and noise in a power supply.
- Chassis mounting, DIN-Rail mount options.
- Applications include industrial automation, HVAC and CNC machines.
M12 PCB/PANEL CONNECTORS 8/12PIN are new plug-in PCB connectors that help to increase production efficiency and decrease installation costs where IP67 protection is required. Suitable for higher signal and data transmission in harsh industrial environments, these high pin density 12-pin connector provides a very compact design with high density connection.
- Plug & play mating for rapid installation.
- Fast and reliable connection for PCB and panel mount.
- 8 and 12 positions
- IP67 with dust-tightness and waterproof to at least 1m.
- Applications include industrial automation, machinery, industrial ethernet and sensors.
Dynamic series connector solutions range from signal level circuitry to power circuit connectivity in a ruggedised, industrialised package. These connectors feature a robust housing structure and high-quality crimp contact system, making them suitable for wire-to-board, wire-to-panel, and wire-to-wire applications in harsh industrial environments.
- Dynamic Mini-Series are low profile connectors for signal transmission on PCB, providing extra board space
- Dynamic D8000 connectors carry currents as high as 100 A per pin for wire-to-wire and 90 A for wire-to-board. They have a rated voltage of 1000V AC/DC and can withstand voltages of up to 3000V AC.
- Dynamic D1000 Series small wire-to-wire connectors are suitable for narrow spaces in small industrial equipment and machinery applications.
For over 75 years, TE Connectivity has partnered with customers to produce highly engineered connectivity and sensing products that make a connected world possible.
The latest new products from TE Connectivity are now available in stock at element14 in APAC.
About us
Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Farnell trades as Farnell in Europe, Newark in North America, and element14 throughout Asia Pacific. Farnell's global businesses are supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Farnell also sells direct to consumers through a network of resellers, and its CPC business in the UK.
Farnell is a business unit of Avnet (Nasdaq: AVT). Avnet is a global technology solutions provider with an extensive ecosystem that delivers design, product, marketing and supply chain expertise for customers at every stage of the lifecycle.
For more information, visit the website at http://www.farnell.com/corporate