London,
17
March
2015
|
00:00
Europe/Amsterdam

element14 Announces Tektronix RF Signal Generator

element14 has introduced the Tektronix TSG4100A series of vector signal generators (VSG) for use in product design, testing and manufacturing.

With the drive towards more affordable test solutions which still meet demanding requirements in wireless design and manufacturing the TSG4100A combines an RF signal generator and a vector signal generator (VSG).  It can be easily upgraded in the field to deliver more advanced vector and digital modulation capabilities.

Priced from £4,190 or $7,300 the TSG4100A series includes three models with carrier frequencies from DC to 2.0 GHz, 4.0 GHz and 6.0 GHz respectively and offer a wide variety of modulation capabilities. Modes include amplitude modulation (AM), frequency modulation (FM), phase modulation (ΦM), and pulse modulation.

Units can be software upgraded to support VSG applications. With the vector upgrade, TSG4100A series offers full support for vector signal modulation on RF carriers between 400 MHz and 6.0 GHz.

The TSG4100A can be used together with the USB-based RSA306 spectrum analyzer, MDO4000B and MDO3000 mixed domain oscilloscopes and is available from Farnell element14 in Europe, Newark element14 in North America and element14 in Asia Pacific.

 

 

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com