element14 launches First Wireless Lab Management Solution for Education from Tektronix

element14 is launching the industry’s first wireless lab instrument management solution from Tektronix, Inc. for quickly setting up and efficiently managing basic electronics engineering laboratories at colleges and universities. The new TekSmartLabTM solution supports up to 120 instruments (30 test benches) on a single platform.
At many education institutions, implementing productive and fully integrated instrument networks in classrooms can be a daunting task. Using LAN cables to set up a network for example is costly, time consuming and limits flexibility and many instruments lack LAN ports. The TekSmartLab eliminates cabling hassles by converting instruments’ USB ports into a wireless interface using a Wi-Fi-USB converter while giving professors the software tools they need to efficiently manage large, busy classrooms.
Priced at £141 for the hardware and £4,240 for the software TekSmartLab eliminates many repetitive manual tasks, saving valuable class time. Features such as intuitive laboratory layout emulation, automatic instrument configuration, and push-button report generation mean that professors and students can focus on learning.
Running on a lab server, TekSmartLab is set up without any LAN cables or special instrument configuration. Professors can load instrument configurations associated with different course requirements and then distribute them to up to 120 instruments with a single mouse click from one central dashboard. Professors can easily check the instrument status and measurement contents of a specific test bench remotely and save student results into a report.
TekSmartLab automatically records and displays asset information and tracks usage time improving overall lab management.
Most Tektronix and Keithley instruments intended for education applications are supported by TekSmartLab including Tektronix TBS1000B-EDU series, DPO/MSO2000B series and MDO3000 series oscilloscopes; AFG2021, AFG1022 and AFG3000C series arbitrary function generators; and Keithley DMM2110 multi-meters and 2231A-30-3 power supplies.
TekSmartLab is available from Farnell element14 in Europe and Newark element14 in North America.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com