London,
01
August
2016
|
01:00
Europe/Amsterdam

TBS2000 oscilloscope from Tektronix brings next generation capabilities to budget constrained design-engineers and educators

New TBS2000 Next Generation Oscillioscope now available at element14

element14 is now stocking the TBS2000 Next Generation Oscilloscope from Tektronix. This new oscilloscope, provides design engineers and educators with an expanded range of capabilities, previously only available in more advanced and expensive models. Based on the proven TDS2000 series, the TBS2000 is the only ‘basic’ model oscilloscope to provide wifi and probe functionality, as well as featuring the longest record length and largest display in its class for faster signal evaluation and troubleshooting.

Increasing accuracy and ease of use for design engineers

Design engineers using oscilloscopes to prototype, debug and validate the designs of new products and for general troubleshooting are increasingly faced with greater signal complexity, tighter signal tolerances and increased time pressure. The functionality of basic equipment currently on the market can lead to a lack of confidence in measurements, and scale factors and corrections continue to be hand-applied due to inability to interface with today’s smart probing technology.

The TBS2000 provides a greater level of functionality than any other basic model oscilloscope.

  • Models are available with 70 MHz or 100 MHz bandwidth and with 2 or 4 channels.

  • Waveform cursor readouts and 32 automatic measurements make it easy to confidently analyze signals.

  • It has the longest record length in its class, at 20M points,

  • The biggest 9 inch WVGA display with 15 horizontal divisions

  • It is the only basic oscilloscope with the TekVPI Probe Interface for better applications coverage with a wider range of active and current probes.

Unique capabilities for enhancing education

For engineering professors, required to teach larger groups of students with an increasing amount of emphasis on hands-on lab work and TBS2000 includes wifi, making it easier to set up an engineering lab, and has a series of built in and online support such as HelpEverywhere and the downloadable Tektronix resource centre to support the teaching of large groups.

 

The new instrument sets a new standard for usability with features like a large display for easy signal visualisation and a comprehensive set of automatic waveform measurements that are coupled with graphical explanations to help engineers better understand their measurements.
Jeff Yost, director, Basic Oscilloscopes, Tektronix
The functionality built into the TBS2000 represents incredible value for money and means that educators looking for ‘real world’ equipment with which to teach can be confident that their purchase will remain relevant as teaching tools for even longer, supporting the education and development of our next generation of engineers.
James McGregor, Global Head of Category – Test and Tools, at element14

element14 offers the latest products, software and solutions from trusted supplier partners through 43 local language transactional websites . The element14 Community allows buyers and engineers to access a wide range of independent technical information, tools and the latest resources and the Design Center enables design engineers to compare kits from the world’s greatest range of development tools.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com