Leeds,
06
April
2022
|
06:30
Europe/Amsterdam

Farnell is now stocking award winning IsoMOV™ protectors from Bourns

Bourns IsoMOV™ hybrid protection component has been singled out as a significant breakthrough in MOV device design.

FAR777 Inline Image

Farnell, an Avnet Company and global distributor of electronic components, products and solutions is now stocking the award winning IsoMOV™ protectors from Bourns.

The innovative hybrid protection component was singled out as a significant breakthrough in MOV device design and won the Electronic Products Passives Product of the Year award in February 2022. This important product introduction further elevates Farnell as a leading distribution partner that offers customers breakthrough products which can solve complex design challenges.

The development of Bourns’ family of IsoMOV™ protectors is one of the most revolutionary technological breakthroughs in overvoltage protection achieved over the last several decades. Applications include electric vehicle charging systems, industrial power supplies, power line communications, high-speed information and communication technology (ICT) equipment, as well as a wide range of certain harsh environment or remote, exposed applications where repairs can be both physically challenging and expensive to perform.

The fully integrated GDT and MOV IsoMOV protector’s hybrid design provides a market leading protection solution that solves MOV failure issues while delivering considerably enhanced surge performance, operational life and device reliability.

Product designers are now able to tailor or upgrade surge protection without having to make performance, size, cost or redesign compromises. IsoMOV™ protectors allow designers to do away with larger, generally lower-performing, and often more expensive surge protection design alternatives.

Bourns is an innovator in device and package design, constantly looking for ways to overcome complex technological problems for customers. Key features of the IsoMOV™ protectors now available from Farnell include:

·       Hybrid protection component integrating the GDT function directly into the MOV itself, providing an elevated level of surge protection performance, operational life and enhanced device reliability. 
·       Combining both devices into a single package allows the GDT to block leakage currents through the MOV that may lead to premature failure, making the MOV inherently more robust without adding additional components into the circuit design. 
·       IsoMOV™ protectors enable designers to better tailor the surge protection performance to their space requirements and allow them to upgrade their MOV overvoltage protection to include the proven benefit of GDT isolation without a PCB redesign. 
·       Industry-standard pin layouts offer a substantial performance and reliability upgrade over same-size standard MOVs in a pin-to-pin drop-in-replacement form factor.

Simon Meadmore, Vice President of Product and Supplier Management at Farnell said “We are delighted that our customers can now purchase Bourns IsoMOV™ protectors from us.  Farnell congratulates the development team for winning this prestigious award and it is great that designers can now get the right level of surge protection for their application without having to make any performance, size, cost or redesign compromises.”

Craig Shipley, Vice President/General Manager of Bourns Circuit Protection Division, said “I commend the entire team that made IsoMOV™ protectors possible and for their success in remedying a complex circuit protection issue for designers. This efficient design gives designers a space-saving, higher performing and generally less expensive option. No longer will engineers have to make trade-offs in order to meet their protection needs.”

He continued “We are very excited to win Product of the Year as it reinforces our drive to provide outstanding value to our customers and enhance their applications today and in the future.”

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in California, USA, Bourns serves a broad range of markets including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio/video and various other market segments.

The IsoMOV™ protectors from Bourns are now available from Farnell in EMEA, Newark in North America and element14 in APAC.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com

Download Media Kit
Download